Import Memory dump into Clock Tree in S32 DS not working!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import Memory dump into Clock Tree in S32 DS not working!

2,688件の閲覧回数
tobiasgrimm
Contributor I

Hello NXP,

i have a BSP38 running on a S32G399 and i want to verifiy the clock settings with S32 DS. I tried to read back a memory dump either in csv or S19 and it is actually not reflecting the values from my dump. I need a Solution really urgent because validations are ongoing, i hope you can support me. I attached the S19 and the CSV Files i tried with.

2024-11-06_18h42_55.png

Best Regards

Tobias

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,644件の閲覧回数
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @tobiasgrimm,

Thanks for contacting NXP support. About your problem, can you elaborate more about it? please share the following information:

  • Which version of the S32 DS are you using?
  • Please describe all the steps you are performing to export and import the register values, what is the expected and the real behavior and please include screenshots when helpful

 

Thanks in advance for the information.

0 件の賞賛
返信

2,617件の閲覧回数
tobiasgrimm
Contributor I

Hello @alejandro_e ,

i am using Build id: 240924 (Update 14) Version 3.5.

I am doing the steps mentioned in your Help section of the Import Register function.

tobiasgrimm_0-1731062880270.png

 

I found out only the format created by the export function can be read in:

ACCEL_PLL->PLLCLKMUX,REFCLKSEL,0
ACCEL_PLL->PLLCR,PLLPD,0
ACCEL_PLL->PLLDV,MFI,80
ACCEL_PLL->PLLDV,RDIV,1
ACCEL_PLL->PLLFD,MFN,0

But actually there is no possibility to import a register dump or something. I need a way to directly import registers from a memory dump or csv file like i attached.

Is there SW Available to create a proper Memory Dump from S32G for the S32DS import function?

Best regards

Tobi

0 件の賞賛
返信

2,604件の閲覧回数
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @tobiasgrimm, 

After exporting to a CSV file, you should be able to import by clicking the import button you show in the image and then selecting the file you exported erlier:

Press the import button:

alejandro_e_0-1731089784614.png

Press the "Browse..." button and search for your file

alejandro_e_1-1731089801954.png

 

Select the file you have exported previously:

alejandro_e_3-1731089911938.png

Once selected click finish:

alejandro_e_4-1731089952324.png

You will see the modified values highlighted in yellow:

alejandro_e_5-1731089973392.png

 

Let me know if you can follow the steps described above or if you encounter any error.

PS: I am not able to see the files you mentioned as attached.

Alejandro

 

 

0 件の賞賛
返信