How to get new activation code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get new activation code?

ソリューションへジャンプ
3,645件の閲覧回数
HyunungPark
Contributor III

I have used S32 design studio for S32K series.

But I download and install a new S32 design studio in addition to S32R series.

I need the activation code for this installation.

How do I get a new activation code?

BRs.

Hyunung 

 

 

0 件の賞賛
返信
1 解決策
3,633件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @HyunungPark ,

The activation code for S32 Design Studio for Power Architecture was provided in the email sent to you. It is the code which begins with '168A'. You can also see this activation code when you login to your account and check the 'license keys' tab when you are on the page for the installation file download.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,634件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @HyunungPark ,

The activation code for S32 Design Studio for Power Architecture was provided in the email sent to you. It is the code which begins with '168A'. You can also see this activation code when you login to your account and check the 'license keys' tab when you are on the page for the installation file download.

Best Regards,

Mike

0 件の賞賛
返信