How to get new activation code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get new activation code?

Jump to solution
3,643 Views
HyunungPark
Contributor III

I have used S32 design studio for S32K series.

But I download and install a new S32 design studio in addition to S32R series.

I need the activation code for this installation.

How do I get a new activation code?

BRs.

Hyunung 

 

 

0 Kudos
Reply
1 Solution
3,631 Views
mikedoidge
NXP Employee
NXP Employee

Hi @HyunungPark ,

The activation code for S32 Design Studio for Power Architecture was provided in the email sent to you. It is the code which begins with '168A'. You can also see this activation code when you login to your account and check the 'license keys' tab when you are on the page for the installation file download.

Best Regards,

Mike

View solution in original post

0 Kudos
Reply
1 Reply
3,632 Views
mikedoidge
NXP Employee
NXP Employee

Hi @HyunungPark ,

The activation code for S32 Design Studio for Power Architecture was provided in the email sent to you. It is the code which begins with '168A'. You can also see this activation code when you login to your account and check the 'license keys' tab when you are on the page for the installation file download.

Best Regards,

Mike

0 Kudos
Reply