How to download the code with S32DS for PA V1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download the code with S32DS for PA V1.1

Jump to solution
2,631 Views
boshimao
Contributor II

Hi NXP
      I want to know how to download the code to flash ?

Labels (2)
0 Kudos
Reply
1 Solution
2,294 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

View solution in original post

0 Kudos
Reply
6 Replies
2,294 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

click Debug icon in the IDE and wait, until code is loaded into the microcontroller.

pastedImage_1.png

Regards,

Martin

0 Kudos
Reply
2,294 Views
boshimao
Contributor II

Hi,

Thank you for your answer, I can understand this, the Debug button can also download the code to the MCU FLASH and RAM, and the RUN button useless. If so, when I do not need to debug function is not too much trouble.

0 Kudos
Reply
2,294 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

RUN button is not implemented in S32 Design Studio. If you need to configure debug settings, click debug configurations and choose the right ones, which are suitable for you. 

pastedImage_1.png

Regards,

Martin

0 Kudos
Reply
2,294 Views
boshimao
Contributor II

Hi

   My debug function is normal. I mean can download code only to flash.

0 Kudos
Reply
2,295 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

0 Kudos
Reply
2,294 Views
boshimao
Contributor II

Hi,

OK,thank you.

0 Kudos
Reply