How to download the code with S32DS for PA V1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download the code with S32DS for PA V1.1

ソリューションへジャンプ
2,447件の閲覧回数
boshimao
Contributor II

Hi NXP
      I want to know how to download the code to flash ?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,110件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,110件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

click Debug icon in the IDE and wait, until code is loaded into the microcontroller.

pastedImage_1.png

Regards,

Martin

0 件の賞賛
返信
2,110件の閲覧回数
boshimao
Contributor II

Hi,

Thank you for your answer, I can understand this, the Debug button can also download the code to the MCU FLASH and RAM, and the RUN button useless. If so, when I do not need to debug function is not too much trouble.

0 件の賞賛
返信
2,110件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

RUN button is not implemented in S32 Design Studio. If you need to configure debug settings, click debug configurations and choose the right ones, which are suitable for you. 

pastedImage_1.png

Regards,

Martin

0 件の賞賛
返信
2,110件の閲覧回数
boshimao
Contributor II

Hi

   My debug function is normal. I mean can download code only to flash.

0 件の賞賛
返信
2,111件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

0 件の賞賛
返信
2,110件の閲覧回数
boshimao
Contributor II

Hi,

OK,thank you.

0 件の賞賛
返信