How do I import the generated code into the s32 development environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I import the generated code into the s32 development environment

ソリューションへジャンプ
2,475件の閲覧回数
niebaochang
Contributor I

I in matable MBD toolbox generates a about mpc5744p single-chip computer code, but I can't put these code successful import S32 development environment, in the process of generating code, I have the target compilers chose S32, but manually import the generated code file will still be a mistakeQQ截图20180718085713.png

タグ(2)
0 件の賞賛
返信
1 解決策
2,308件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

There is already a great article on this.

https://community.nxp.com/message/925216 

Hope it helps,

Mike

元の投稿で解決策を見る

2 返答(返信)
2,309件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

There is already a great article on this.

https://community.nxp.com/message/925216 

Hope it helps,

Mike

2,308件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

in my opinion you are facing standard C issues - like missing headers, missing path to headers and So on. Just make sure that you have set all include paths correctly and project contains all necessary headers. 

Jiri

0 件の賞賛
返信