How can I download my code to the flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I download my code to the flash?

ソリューションへジャンプ
2,956件の閲覧回数
578294688
Contributor II

Hello!

I want to know which tool I should use to download the program?JTAG?Or others?

My chip is S32R274.

I looking forward to your reply.

Thank you!

0 件の賞賛
返信
1 解決策
2,772件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,773件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

0 件の賞賛
返信
2,772件の閲覧回数
578294688
Contributor II

I have saw that the chip have the interface of JTAG,can I use the JTAG to download my code to the flash and debug?

Thank you !

0 件の賞賛
返信
2,772件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes - the probes mentioned above are connected via JTAG.

Jiri

0 件の賞賛
返信
2,772件の閲覧回数
578294688
Contributor II

OK,thank for your help,Jiri!

Thanks!Thanks!

0 件の賞賛
返信