How can I download my code to the flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I download my code to the flash?

跳至解决方案
2,151 次查看
578294688
Contributor II

Hello!

I want to know which tool I should use to download the program?JTAG?Or others?

My chip is S32R274.

I looking forward to your reply.

Thank you!

0 项奖励
回复
1 解答
1,967 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,968 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

0 项奖励
回复
1,967 次查看
578294688
Contributor II

I have saw that the chip have the interface of JTAG,can I use the JTAG to download my code to the flash and debug?

Thank you !

0 项奖励
回复
1,967 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes - the probes mentioned above are connected via JTAG.

Jiri

0 项奖励
回复
1,967 次查看
578294688
Contributor II

OK,thank for your help,Jiri!

Thanks!Thanks!

0 项奖励
回复