How can I download my code to the flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I download my code to the flash?

Jump to solution
2,928 Views
578294688
Contributor II

Hello!

I want to know which tool I should use to download the program?JTAG?Or others?

My chip is S32R274.

I looking forward to your reply.

Thank you!

0 Kudos
Reply
1 Solution
2,744 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

View solution in original post

0 Kudos
Reply
4 Replies
2,745 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the low cost solution is PE Micro USB Multilink probe and the high end is Lauterbach debugger. Probably the PE Micro is good choice for you and is working okay. 

Jiri 

0 Kudos
Reply
2,744 Views
578294688
Contributor II

I have saw that the chip have the interface of JTAG,can I use the JTAG to download my code to the flash and debug?

Thank you !

0 Kudos
Reply
2,744 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes - the probes mentioned above are connected via JTAG.

Jiri

0 Kudos
Reply
2,744 Views
578294688
Contributor II

OK,thank for your help,Jiri!

Thanks!Thanks!

0 Kudos
Reply