GPCLR GPCHR value issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPCLR GPCHR value issue

2,350件の閲覧回数
samcs
Contributor II

I debugged a program, at breakpoint, i got.

Debug1.png

GPCLR,GPCHR value is 0x80008000(2147516416), looked through the code, can't find where is the 0x80008000 from, it's global ,should be set to 0.

0 件の賞賛
返信
3 返答(返信)

2,334件の閲覧回数
samcs
Contributor II

And I found at breakpoint rtos_start(), the GPCLR,GPCHR value is also 0x80008000 too.

PCR[0]..PCR[31] , be set to 0x80008000 (2147516416) too, seems default value is not zero, is 0x80008000.

0 件の賞賛
返信

2,323件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Sam,

first of all, which device and which SDK/RTD do you have?

Regards,

Lukas

0 件の賞賛
返信

2,298件の閲覧回数
samcs
Contributor II

It's clock cofiguration issue,fixed

0 件の賞賛
返信