GPCLR GPCHR value issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPCLR GPCHR value issue

1,637 次查看
samcs
Contributor II

I debugged a program, at breakpoint, i got.

Debug1.png

GPCLR,GPCHR value is 0x80008000(2147516416), looked through the code, can't find where is the 0x80008000 from, it's global ,should be set to 0.

0 项奖励
回复
3 回复数

1,621 次查看
samcs
Contributor II

And I found at breakpoint rtos_start(), the GPCLR,GPCHR value is also 0x80008000 too.

PCR[0]..PCR[31] , be set to 0x80008000 (2147516416) too, seems default value is not zero, is 0x80008000.

0 项奖励
回复

1,610 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Sam,

first of all, which device and which SDK/RTD do you have?

Regards,

Lukas

0 项奖励
回复

1,585 次查看
samcs
Contributor II

It's clock cofiguration issue,fixed

0 项奖励
回复