Flash Configuration option missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Configuration option missing

1,490 Views
ameershira
Contributor I

In "HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio" a Flash Configuration option under option 1 to flash a MCU with a compiled binary.

This option however seems to be missing in the version of Design Studio I'm using:

S32 Design Studio for S32 Platform
Build id: 201217 (Update 3)

OS: Windows 10, v.10.0, x86_64 / win32
Java version: 1.8.0_202

0 Kudos
Reply
1 Reply

1,483 Views
mikedoidge
NXP Employee
NXP Employee

Hello Ameer,

You are correct. The article  HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio is for use with S32 Design Studio for Arm or S32 Design Studio for Power Architecture. It is not applicable to S32 Design Studio for S32 Platform.

To flash an executable to target for S32 Design Studio for S32 Platform you have options:

1) S32 Debugger Flash Programmer

2) S32 Flash Tool

3) PE Micro GDB (for S32K1 family)

Best Regards,

Mike

0 Kudos
Reply