Flash Configuration option missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Configuration option missing

1,514件の閲覧回数
ameershira
Contributor I

In "HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio" a Flash Configuration option under option 1 to flash a MCU with a compiled binary.

This option however seems to be missing in the version of Design Studio I'm using:

S32 Design Studio for S32 Platform
Build id: 201217 (Update 3)

OS: Windows 10, v.10.0, x86_64 / win32
Java version: 1.8.0_202

0 件の賞賛
返信
1 返信

1,507件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Ameer,

You are correct. The article  HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio is for use with S32 Design Studio for Arm or S32 Design Studio for Power Architecture. It is not applicable to S32 Design Studio for S32 Platform.

To flash an executable to target for S32 Design Studio for S32 Platform you have options:

1) S32 Debugger Flash Programmer

2) S32 Flash Tool

3) PE Micro GDB (for S32K1 family)

Best Regards,

Mike

0 件の賞賛
返信