FLASH FROM FILE QUESTION?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLASH FROM FILE QUESTION?

Jump to solution
3,681 Views
frank_feng
Contributor II

S32DS-1.PNG

why the repository of flashfromfile is not available ?

Labels (1)
0 Kudos
Reply
1 Solution
3,522 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

View solution in original post

3 Replies
3,522 Views
frank_feng
Contributor II

Hi,

Thank you for your answering .

I have another question about the demos supported in the S32DS for Vision .

Recently ,I am going to use the M4 core existed in S32V234 to develop some applications surrounded with can interface and uart interface  on S32V234-EVB ,However , I could only find one simple demo named m4_boot_flash ,I wonder if it is possible to support me with more M4 bareboard demos  about the can interface and uart interface , I really need these demos , if you have or know how to get these demos , please let me know , I'll be very thankful !

Thank you  

0 Kudos
Reply
3,523 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

3,522 Views
elorlova6
Contributor I

@Jiri Kral

Thank you so much for the suggestion. I'm also confused... myprepaidcenter card

0 Kudos
Reply