FLASH FROM FILE QUESTION?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLASH FROM FILE QUESTION?

ソリューションへジャンプ
3,667件の閲覧回数
frank_feng
Contributor II

S32DS-1.PNG

why the repository of flashfromfile is not available ?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,508件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

元の投稿で解決策を見る

3 返答(返信)
3,508件の閲覧回数
frank_feng
Contributor II

Hi,

Thank you for your answering .

I have another question about the demos supported in the S32DS for Vision .

Recently ,I am going to use the M4 core existed in S32V234 to develop some applications surrounded with can interface and uart interface  on S32V234-EVB ,However , I could only find one simple demo named m4_boot_flash ,I wonder if it is possible to support me with more M4 bareboard demos  about the can interface and uart interface , I really need these demos , if you have or know how to get these demos , please let me know , I'll be very thankful !

Thank you  

0 件の賞賛
返信
3,509件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

3,508件の閲覧回数
elorlova6
Contributor I

@Jiri Kral

Thank you so much for the suggestion. I'm also confused... myprepaidcenter card

0 件の賞賛
返信