FLASH FROM FILE QUESTION?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FLASH FROM FILE QUESTION?

跳至解决方案
3,807 次查看
frank_feng
Contributor II

S32DS-1.PNG

why the repository of flashfromfile is not available ?

标签 (1)
0 项奖励
回复
1 解答
3,648 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

在原帖中查看解决方案

3 回复数
3,648 次查看
frank_feng
Contributor II

Hi,

Thank you for your answering .

I have another question about the demos supported in the S32DS for Vision .

Recently ,I am going to use the M4 core existed in S32V234 to develop some applications surrounded with can interface and uart interface  on S32V234-EVB ,However , I could only find one simple demo named m4_boot_flash ,I wonder if it is possible to support me with more M4 bareboard demos  about the can interface and uart interface , I really need these demos , if you have or know how to get these demos , please let me know , I'll be very thankful !

Thank you  

0 项奖励
回复
3,648 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this feature is not supported in S32DS for Vision. 

Jiri

3,648 次查看
elorlova6
Contributor I

@Jiri Kral

Thank you so much for the suggestion. I'm also confused... myprepaidcenter card

0 项奖励
回复