Errors in peripheral configuration after importing S32K3 T-Box BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errors in peripheral configuration after importing S32K3 T-Box BSP

Jump to solution
980 Views
hns80
Contributor V

I am using S32DS 3.4 and installed SW32K3_RTD_4.4_1.0.0_HF02_DS_updatesite_D2112, then imported (File->Import->Existing projects into workspace)  the S32K3_T_BOX_BSP.zip project.

While the project appears to import fine, the peripheral configurator shows many errors.

hns80_0-1686838429080.png

Is this common? Is there something I should be doing differently?

 

 

Tags (1)
0 Kudos
Reply
1 Solution
950 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@hns80

the SDK you're using is RTD 2.0.0,not RTD 1.0.0

Senlent_0-1687158230522.png

This is a known tool bug, please try the following.

"If you installed both RTD RTM 1.0.0 and RTM 2.0.0. to avoid project RTD version auto conversion which would break up the old version projects, try to remove the "compatibility.xml" located at "

C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration

"

 

View solution in original post

0 Kudos
Reply
1 Reply
951 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@hns80

the SDK you're using is RTD 2.0.0,not RTD 1.0.0

Senlent_0-1687158230522.png

This is a known tool bug, please try the following.

"If you installed both RTD RTM 1.0.0 and RTM 2.0.0. to avoid project RTD version auto conversion which would break up the old version projects, try to remove the "compatibility.xml" located at "

C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration

"

 

0 Kudos
Reply