Errors in peripheral configuration after importing S32K3 T-Box BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Errors in peripheral configuration after importing S32K3 T-Box BSP

跳至解决方案
976 次查看
hns80
Contributor V

I am using S32DS 3.4 and installed SW32K3_RTD_4.4_1.0.0_HF02_DS_updatesite_D2112, then imported (File->Import->Existing projects into workspace)  the S32K3_T_BOX_BSP.zip project.

While the project appears to import fine, the peripheral configurator shows many errors.

hns80_0-1686838429080.png

Is this common? Is there something I should be doing differently?

 

 

标记 (1)
0 项奖励
回复
1 解答
946 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@hns80

the SDK you're using is RTD 2.0.0,not RTD 1.0.0

Senlent_0-1687158230522.png

This is a known tool bug, please try the following.

"If you installed both RTD RTM 1.0.0 and RTM 2.0.0. to avoid project RTD version auto conversion which would break up the old version projects, try to remove the "compatibility.xml" located at "

C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration

"

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
947 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@hns80

the SDK you're using is RTD 2.0.0,not RTD 1.0.0

Senlent_0-1687158230522.png

This is a known tool bug, please try the following.

"If you installed both RTD RTM 1.0.0 and RTM 2.0.0. to avoid project RTD version auto conversion which would break up the old version projects, try to remove the "compatibility.xml" located at "

C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration

"

 

0 项奖励
回复