Error while running the program in S32 Design Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error while running the program in S32 Design Studio

1,433 次查看
Krishna_Yalamanchili
Contributor I

Hi,

I am getting the following error when Run is pressed in S32 Design studio. I am trying to run after debug file is flashed and run. Please suggest what I have to do if i have to run the application only.

Error starting process.
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed

0 项奖励
回复
1 回复

1,389 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @Krishna_Yalamanchili,

Are you trying to just run or also debug?

If the application has been flashed successfully, then you just cycle the power to the board and it should run.

Best Regards,

Mike

0 项奖励
回复