Download timer too long

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download timer too long

2,199 Views
chenxiubo
Contributor III

Hi,

       I'm using mpc5748g, PE and S32DS V1.1, I downloaded the project  need 3~4 minutes, it's too long time. Is there any 

configuration to download the code using fewer time?

0 Kudos
Reply
2 Replies

2,067 Views
stanish
NXP Employee
NXP Employee

Hello Chen,

Thanks for this report!

This is a known issue that has been fixed in the latest version of S32DS for Power:S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released!

Therefore I'd recommend you to download and install it.

Note: You can have multiple versions of S32DS installed on the same machine.

Stan

0 Kudos
Reply

2,067 Views
chenxiubo
Contributor III

Hi,Stan

   

           I tested my project:  In the S32DS V2.0, it costed about 70 seconds(if clean the project and build, about 100 seconds). In the S32DS V1.1, it costed about 180 seconds(if clean the project and build, about 245 seconds).

      

          

0 Kudos
Reply