Debugging an application in S32 IDE not working as expected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging an application in S32 IDE not working as expected

ソリューションへジャンプ
4,719件の閲覧回数
p070042
Contributor III

Hi, I have started debugging an application in S32 IDE, After getting stop in main function, When I do step in, It directly jumps to some task even without initializing & starting OS. 

Below is the code which I am trying to debug. When i start debugging, Breakpoints hits the main function & on very next step in, instead of going function CPU_IntDis(), It directly hits the some task. Which I think should only be started when scheduler will schedule it.

int main(void) {
OS_ERR osErr;
ERR_E err;

//disable all interrupts
CPU_IntDis();

INIT_sysClk(&err);
if (err != ERR_OK) {
while(TRUE);
}
OSInit(&osErr);
SCHTask_init();
OSStart(&osErr);

while(TRUE);
return 0;
}

0 件の賞賛
返信
1 解決策
4,093件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details: https://community.nxp.com/docs/DOC-335361 

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,093件の閲覧回数
p070042
Contributor III

Hi,

   I am using MPC5744 & Version of S32 DS is 1.2

0 件の賞賛
返信
4,094件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details: https://community.nxp.com/docs/DOC-335361 

Jiri

0 件の賞賛
返信
4,093件の閲覧回数
p070042
Contributor III

Hi,

    Thanks very much. Really cool :smileyhappy: 

It solved my issue. 

0 件の賞賛
返信
4,093件の閲覧回数
p070042
Contributor III

Hi,

Yes, You are absolutely right, The actual project was created for older version v1.1 and I have imported it in V1.2 and tried to debug it. Yes, this can be the issue. 

0 件の賞賛
返信
4,093件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your MCU and which version of S32DS are you using? 

Jiri

0 件の賞賛
返信