Debugging an application in S32 IDE not working as expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging an application in S32 IDE not working as expected

Jump to solution
4,844 Views
p070042
Contributor II

Hi, I have started debugging an application in S32 IDE, After getting stop in main function, When I do step in, It directly jumps to some task even without initializing & starting OS. 

Below is the code which I am trying to debug. When i start debugging, Breakpoints hits the main function & on very next step in, instead of going function CPU_IntDis(), It directly hits the some task. Which I think should only be started when scheduler will schedule it.

int main(void) {
OS_ERR osErr;
ERR_E err;

//disable all interrupts
CPU_IntDis();

INIT_sysClk(&err);
if (err != ERR_OK) {
while(TRUE);
}
OSInit(&osErr);
SCHTask_init();
OSStart(&osErr);

while(TRUE);
return 0;
}

0 Kudos
Reply
1 Solution
4,218 Views
jiri_kral
NXP Employee
NXP Employee

Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details: https://community.nxp.com/docs/DOC-335361 

Jiri

View solution in original post

0 Kudos
Reply
5 Replies
4,218 Views
p070042
Contributor II

Hi,

   I am using MPC5744 & Version of S32 DS is 1.2

0 Kudos
Reply
4,219 Views
jiri_kral
NXP Employee
NXP Employee

Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details: https://community.nxp.com/docs/DOC-335361 

Jiri

0 Kudos
Reply
4,218 Views
p070042
Contributor II

Hi,

    Thanks very much. Really cool :smileyhappy: 

It solved my issue. 

0 Kudos
Reply
4,218 Views
p070042
Contributor II

Hi,

Yes, You are absolutely right, The actual project was created for older version v1.1 and I have imported it in V1.2 and tried to debug it. Yes, this can be the issue. 

0 Kudos
Reply
4,218 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your MCU and which version of S32DS are you using? 

Jiri

0 Kudos
Reply