Cannot run program "make.exe"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot run program "make.exe"

Jump to solution
2,692 Views
RobertKhan
Contributor I

Good day!

Recently my system (Windows 10) got updated and S32 DS for ARM 2.2 doesn't work anymore, showing this problem:

Cannot run program "C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\msys32\usr\bin\make.exe": ?? ??????? ????? ????????? ????.

Of course I have checked whether the make tool exists in the folder above and whether it works. Everything is fine here.

I also have checked system environments and added these paths:

C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\msys32\usr\bin

C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v6.3\gcc-6.3-arm32-eabi\bin

After that I moved to my project's Debug folder and tried to call make inside of this folder. Everything was built without any problems.

But S32 DS itself still shows this error and does nothing. I also tried reinstall it several times, but it didn't help. I have attached screenshot of this error:

Spoiler
error.png

 

0 Kudos
Reply
1 Solution
2,608 Views
RobertKhan
Contributor I

Well, I tried dozens of different solutions and none of them helped me. So I reinstalled Windows and error has gone (I hope forever). Hate buggy Windows and Eclipse based IDEs.

The question can be closed now, no one will answer anyway.

View solution in original post

0 Kudos
Reply
1 Reply
2,609 Views
RobertKhan
Contributor I

Well, I tried dozens of different solutions and none of them helped me. So I reinstalled Windows and error has gone (I hope forever). Hate buggy Windows and Eclipse based IDEs.

The question can be closed now, no one will answer anyway.

0 Kudos
Reply