Cannot run program "make.exe"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot run program "make.exe"

ソリューションへジャンプ
2,695件の閲覧回数
RobertKhan
Contributor I

Good day!

Recently my system (Windows 10) got updated and S32 DS for ARM 2.2 doesn't work anymore, showing this problem:

Cannot run program "C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\msys32\usr\bin\make.exe": ?? ??????? ????? ????????? ????.

Of course I have checked whether the make tool exists in the folder above and whether it works. Everything is fine here.

I also have checked system environments and added these paths:

C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\msys32\usr\bin

C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v6.3\gcc-6.3-arm32-eabi\bin

After that I moved to my project's Debug folder and tried to call make inside of this folder. Everything was built without any problems.

But S32 DS itself still shows this error and does nothing. I also tried reinstall it several times, but it didn't help. I have attached screenshot of this error:

スポイラ
error.png

 

0 件の賞賛
返信
1 解決策
2,611件の閲覧回数
RobertKhan
Contributor I

Well, I tried dozens of different solutions and none of them helped me. So I reinstalled Windows and error has gone (I hope forever). Hate buggy Windows and Eclipse based IDEs.

The question can be closed now, no one will answer anyway.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,612件の閲覧回数
RobertKhan
Contributor I

Well, I tried dozens of different solutions and none of them helped me. So I reinstalled Windows and error has gone (I hope forever). Hate buggy Windows and Eclipse based IDEs.

The question can be closed now, no one will answer anyway.

0 件の賞賛
返信