Can not create project from example in S32DS for S32K344EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can not create project from example in S32DS for S32K344EVB

695 次查看
kk2023
Contributor I

The installed Extensions is shown in the following figure:

kk2023_0-1719099264423.png

However, when I create project from example, in the project's includes path the 'generate' and 'RTD' path is grayed out. And the project can not compile properly. As shown in the following figure. So, what's wrong with the Create project from Example in S32DS?

kk2023_3-1719099649504.png

 

kk2023_1-1719099494311.png

kk2023_2-1719099550332.png

 

0 项奖励
回复
1 回复

660 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @kk2023 

Before running any example code, it is required to generate the project configurations.
Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Clocks, Peripherals, etc...). Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the "S32 Configuration Tool > Update Code" button.

 

B.R.

VaneB

0 项奖励
回复