Can not create project from example in S32DS for S32K344EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not create project from example in S32DS for S32K344EVB

704 Views
kk2023
Contributor I

The installed Extensions is shown in the following figure:

kk2023_0-1719099264423.png

However, when I create project from example, in the project's includes path the 'generate' and 'RTD' path is grayed out. And the project can not compile properly. As shown in the following figure. So, what's wrong with the Create project from Example in S32DS?

kk2023_3-1719099649504.png

 

kk2023_1-1719099494311.png

kk2023_2-1719099550332.png

 

0 Kudos
Reply
1 Reply

669 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @kk2023 

Before running any example code, it is required to generate the project configurations.
Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Clocks, Peripherals, etc...). Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the "S32 Configuration Tool > Update Code" button.

 

B.R.

VaneB

0 Kudos
Reply