CAN configuration for s32K324

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN configuration for s32K324

5,149 次查看
LavanyaR
Contributor I

Hi,

Here we are working in s32k324. We tried s32k312 CAN example code configuration into s32k324. But it is not working. If you CAN driver code for s32k324 means kindly share it to us.

 

Thank you in advance

0 项奖励
回复
14 回复数

5,085 次查看
Riyasma07
Contributor III

Hi @VaneB,

I've entered the following values for FlexCAN bitrate configuration and updated the code.

Riyasma07_0-1702881790228.png

But the code does not get updated. Old config values are still there in the FlexCAN_Config0 structure variable. But other parameter values are gets updated.

Riyasma07_1-1702881968539.png

I'm using RTD V3.0.0

Please check and update.

 

0 项奖励
回复

5,040 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Riyasma07 

Please check the following post. Here, I am helping another customer with the same situation. 

The S32DS peripheral configuration tool for the S32 platform fails to generate a configuration file

 

B.R.

VaneB

0 项奖励
回复

5,131 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

Sorry for the inconvenience this might cause. 

We do not have an example for S32K324, but you can use the available ones for S32K344 devices (included with the RTDs). 

Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200

As you can see in the following image, the S32K344 is pin-to-pin compatible with S32K324. So it is easier to port the examples to the MCU you are using. 

VaneB_0-1702668074585.png

 

B.R.

VaneB

4,608 次查看
LavanyaR
Contributor I

Hi @VaneB 

Shall we use s32k344 example driver code for s32k322 microcontroller? or Do you have driver code for s32k322 microcontroller

0 项奖励
回复

4,598 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

I will be helping you with this topic in this post (Driver configuration for S32K322). 

0 项奖励
回复

5,087 次查看
LavanyaR
Contributor I

Hello all,

I have tried this code for s32k324 but this is also not working. Same s32k344 code we checked in Evolution Board. It send the data in one time. In s32k324 controller CAN code not working and producing Bus error. Kindly give the clarification for CAN configuration. 

Thanks you in advance

0 项奖励
回复

5,042 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

Could you share an image of the error you are getting? Also, could you provide more details about the project's behavior?

0 项奖励
回复

5,021 次查看
LavanyaR
Contributor I

Hi @VaneB 

Screenshot 2023-12-19 095350.png

I have checked Loop-back mode and Normal mode. But we are receiving the 

Bus Error. And i don't have the clarity about those mode. Kindly explain about the modes and which mode need to choose.

0 项奖励
回复

4,976 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

Sorry for the inconvenience this might cause. I am not familiar with the tool you are using. 

Also, the CAN_Example was developed as a LoopBack example, so no external tools or external connections are needed. 

0 项奖励
回复

4,889 次查看
LavanyaR
Contributor I

Hi @VaneB 

In Example code clock configuration have the below options are enabled.

LavanyaR_0-1703387361773.png

If i enabled these options means whether it occur  hard fault error or get stuck in below condition.

LavanyaR_1-1703387648075.png

 

 

 

0 项奖励
回复

4,849 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

The function Clock_Ip_GetClockFrequency returns the frequency of a given clock, in this case, FXOSC. Make sure that the clock configuration on Config Tools has the same value as your external clock/oscillator. 

 

0 项奖励
回复

4,811 次查看
LavanyaR
Contributor I

Hi @VaneB 

In FXOSC and CAN0 to CAN5 having the same frequency. I have configures as 16MHz.

LavanyaR_0-1703651362897.png

 

LavanyaR_1-1703651390524.png

 

0 项奖励
回复

4,780 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @LavanyaR 

Could you share your example project so I can test it from my side? Or, if it is not possible, could you share all the configurations made in COnfigTools? So I can try to replicate the problem using an example code.

0 项奖励
回复

4,719 次查看
LavanyaR
Contributor I

Hi @VaneB 

CAN driver is working now.

Thank you

0 项奖励
回复