Bug: Processor Expert fails on startup if no configuration is enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug: Processor Expert fails on startup if no configuration is enabled

1,093件の閲覧回数
janijärvenpää
Contributor II

Hi, I  removed two configurations on processor expert (i had duplicate debug ram and debug flash configurations). I closed and restarted S32DS and i noticed that my Components view was not visible.  After clicking ProcessorExpert.pe on project explorer, the whole IDE goes stuck, and does not respond.

After a bit of troubleshooting, i compared older version to current version of ProcessorExpert.pe, i noticed that there was  <CnfgEnabled>false</CnfgEnabled> on both configurations. I set CnfgEnabled to true on debug ram configuration, and restarted S32DS and everything was running fine again.

Steps to reproduce:

-Edit CnfgEnabled XML elements value to false on all configurations. 

-Start S32 design studio

-click ProcessorExpert.pe on project explorer

Version info

S32 Design Studio For ARM

Version: 2018.R1
Build id: 180815

Have a nice day!

-Jani

タグ(2)
0 件の賞賛
返信
1 返信

1,021件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried to reproduce this issue with latest S32DS Version (v2.1.) and it looks that this issue is already fixed. Thanks for report. 

Jiri 

0 件の賞賛
返信