Basic example project file for GHS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic example project file for GHS

2,628 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

Could I get an basic example project file for GHS with S32K14x? 

Best regards,

Kate Lee

Labels (1)
0 Kudos
Reply
2 Replies

2,459 Views
mikedoidge
NXP Employee
NXP Employee

Hi Kate,

You will first need to contact Green Hills to get the Eclipse Neon compatible plug-in. Then, after you install the plug-in, you should be able to use the New Project from Example wizard to see the Hello World example included in the SDK. Alternatively, you could use the New Project Wizard to create an empty project.

Best Regards,

Mike

0 Kudos
Reply

2,459 Views
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

unfortunately I don't have any GHS examples for S32K144 - hope that someone on community will share something. 

Jiri 

0 Kudos
Reply