S32DS for Vision contains many example projects from which you can learn how S32DS for Vision can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS for Vision. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed.
1) Launch S32DS for Vision
2) Select "New S32DS Project from example"
3) Select isp_sonyimx224_csi_dcu project
In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_sonyimx224_csi_dcu_graph'. Then double click on 'ISP data flow : isp_sonyimx224_csi_dcu_graph'. The ISP graph diagram will appear in the editor panel.
4) Change to C/C++ perspective, click on 'Switch to C/C++ Development'
5) Select isp_sonyimx224_csi_dcu: A53 in the Project Explorer panel
6) Build project for A53
7) Start a debug session using method as described in HOWTO Create A53 Linux Project in S32DS for Vision, beginning at step 9.
8) Should get results similar to this:
Hi Mike Doidge
It is helpful when i follow your guide to create project. But i encounter a strange issue. Could you help me for this? Thanks.
My S32 DS is :S32 Design Studio for Vision Version 2018.R1
PC OS version: ubuntu 14.04 64bits
When i build the project, the logs shown as below:
13:42:02 **** Build of configuration A53 for project isp_sonyimx224_csi_dcu ****
make -j4 all
make --no-print-directory pre-build
rm -f ../A53_gen/src/sequencer_srec.c; make -f ../Project_Settings/Scripts/seq.mk TD="/root/NXP/S32DS_Vision_v2018.R1/eclipse/../Cross_Tools/gcc-6.3-arm32-eabi" VD="/root/NXP/S32DS_Vision_v2018.R1/eclipse/../S32DS/s32v234_sdk"
make[2]: dos2unix: Command not found
make --no-print-directory main-build
Building file: ../A53_src/main.cpp
Invoking: Standard S32DS C++ Compiler
aarch64-linux-gnu-g++ "@A53_src/main.args" -MMD -MP -MF"A53_src/main.d" -MT"A53_src/main.o" -o "A53_src/main.o" "../A53_src/main.cpp"
make[2]: *** [../A53_gen/src/sequencer_srec.c] Error 127
make[1]: [pre-build] Error 2 (ignored)
Building file: ../A53_gen/src/kmem.c
Building file: ../A53_gen/src/mipi_simple.c
Invoking: Standard S32DS C Compiler
aarch64-linux-gnu-gcc "@A53_gen/src/kmem.args" -MMD -MP -MF"A53_gen/src/kmem.d" -MT"A53_gen/src/kmem.o" -o "A53_gen/src/kmem.o" "../A53_gen/src/kmem.c"
Invoking: Standard S32DS C Compiler
aarch64-linux-gnu-gcc "@A53_gen/src/kmem.args" -MMD -MP -MF"A53_gen/src/mipi_simple.d" -MT"A53_gen/src/mipi_simple.o" -o "A53_gen/src/mipi_simple.o" "../A53_gen/src/mipi_simple.c"
Finished building: ../A53_gen/src/kmem.c
Finished building: ../A53_gen/src/mipi_simple.c
Finished building: ../A53_src/main.cpp
Building target: s32ds_isp_sonyimx224_csi_dcu.elf
Invoking: Standard S32DS C++ Linker
aarch64-linux-gnu-g++ -o "s32ds_isp_sonyimx224_csi_dcu.elf" "@s32ds_isp_sonyimx224_csi_dcu.args"
./A53_src/main.o: In function `LibsPrepare(AppContext&)':
/root/workspaceS32DS.Vision.2018.R1/isp_sonyimx224_csi_dcu/isp_sonyimx224_csi_dcu/A53/../A53_src/main.cpp:298: undefined reference to `sequencer_srec'
/root/workspaceS32DS.Vision.2018.R1/isp_sonyimx224_csi_dcu/isp_sonyimx224_csi_dcu/A53/../A53_src/main.cpp:298: undefined reference to `sequencer_srec'
collect2: error: ld returned 1 exit status
make[1]: *** [s32ds_isp_sonyimx224_csi_dcu.elf] Error 1
make: *** [all] Error 2
13:42:07 Build Finished (took 4s.477ms)
Description Resource Path Location Type
Ld error: 2 (ignored) C/C++ Problem
Ld error: 2 (ignored) C/C++ Problem
Ld error: undefined reference to `sequencer_srec' isp_sonyimx224_csi_dcu C/C++ Problem
make: *** [all] Error 2 isp_sonyimx224_csi_dcu C/C++ Problem
make[1]: *** [s32ds_isp_sonyimx224_csi_dcu.elf] Error 1 isp_sonyimx224_csi_dcu C/C++ Problem
make[2]: *** [../A53_gen/src/sequencer_srec.c] Error 127 isp_sonyimx224_csi_dcu C/C++ Problem