eeprom does retains the data afterresetMM9Z1I638

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eeprom does retains the data afterresetMM9Z1I638

ソリューションへジャンプ
1,634件の閲覧回数
lahcenmejjad
Contributor I

Hi,

I am using the sample code provide by Freescale(NXP) in the project KT9Z1-638-REFAPP.

The Eeprom erased when I reset or power off  the board. 

I  am using the function, EEPROM_WriteCalibValue as it is.

best regards

0 件の賞賛
返信
1 解決策
1,576件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

If the EEPROM is erased, there must be a function that erases it.

Have you tried to halt the execution just after POR, check the EEPROM and step the code?

Thanks,

BR, Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,577件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

If the EEPROM is erased, there must be a function that erases it.

Have you tried to halt the execution just after POR, check the EEPROM and step the code?

Thanks,

BR, Daniel

0 件の賞賛
返信
1,576件の閲覧回数
lahcenmejjad
Contributor I

Hello Daniel,

thank you for your response,

I did step by step , but I was using library  from NXP ( executable code), so I could not go through their code.when I replaced the CPU, and It seems every thing is working fine  so far.

I think the problem is resolved !!

0 件の賞賛
返信