automotive qualified

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

automotive qualified

3,508件の閲覧回数
Ahmeduchi
Contributor I

Dear All,

I want to ask about NXP parts that begin with S9 prefix .

are all automotive qualified according to AEC-Q100 ?!

0 件の賞賛
返信
3 返答(返信)

3,489件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Dear Ahmeduchi,

 

Since the area of MCUs which starts with "S9" is huge and there are, also, MCUs that are qualified according to AEC-Q100 and part numbers do not begin with "S9". Could you please, specify the area of MCUs you are interested in?

Thank you.

Best regards,

Diana

0 件の賞賛
返信

3,463件の閲覧回数
Ahmeduchi
Contributor I

Hi Diana,

Thank you very much to follow up with my request .

Can you please see attached MCUs which I am interested in to give me the automotive qualified ones to AEC-Q100  .

 

Thanks,

Ahmed Alaa

Senior Design Engineer

0 件の賞賛
返信

3,427件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Ahmed,

 

I have checked your list and I'm focused on 16-bit MCUs (S12(X), MagniV):

The 16-bit MCUs which starts with S9 are automotive qualified. However, it is not easy to check AEC- Q100 certification for all MCUs which you have on the list. In general, all of these parts should be AEC qualified. But if you want to check the AEC-Q100 certification, please, pick just a few of them.

For the MCUs with different areas such as Kinetis and 8-bit from your list, please, create a new request to the related community:

https://community.nxp.com/t5/8-bit-Microcontrollers/bd-p/8bit

https://community.nxp.com/t5/Kinetis-Microcontrollers/bd-p/kinetis

 

Best regards,

Diana

0 件の賞賛
返信