automotive qualified

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

automotive qualified

3,509 Views
Ahmeduchi
Contributor I

Dear All,

I want to ask about NXP parts that begin with S9 prefix .

are all automotive qualified according to AEC-Q100 ?!

0 Kudos
Reply
3 Replies

3,490 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Dear Ahmeduchi,

 

Since the area of MCUs which starts with "S9" is huge and there are, also, MCUs that are qualified according to AEC-Q100 and part numbers do not begin with "S9". Could you please, specify the area of MCUs you are interested in?

Thank you.

Best regards,

Diana

0 Kudos
Reply

3,464 Views
Ahmeduchi
Contributor I

Hi Diana,

Thank you very much to follow up with my request .

Can you please see attached MCUs which I am interested in to give me the automotive qualified ones to AEC-Q100  .

 

Thanks,

Ahmed Alaa

Senior Design Engineer

0 Kudos
Reply

3,428 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Ahmed,

 

I have checked your list and I'm focused on 16-bit MCUs (S12(X), MagniV):

The 16-bit MCUs which starts with S9 are automotive qualified. However, it is not easy to check AEC- Q100 certification for all MCUs which you have on the list. In general, all of these parts should be AEC qualified. But if you want to check the AEC-Q100 certification, please, pick just a few of them.

For the MCUs with different areas such as Kinetis and 8-bit from your list, please, create a new request to the related community:

https://community.nxp.com/t5/8-bit-Microcontrollers/bd-p/8bit

https://community.nxp.com/t5/Kinetis-Microcontrollers/bd-p/kinetis

 

Best regards,

Diana

0 Kudos
Reply