XGATE on MC9S12XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XGATE on MC9S12XEP100

1,619 Views
lubošvidner
Contributor I

Hello

Please


I would like to put XGATE on  MC9S12XEP100. After the net, I tried to find out some code, for example on the topic of transmitting the character after sci.  I tried some of the codes, but it was only in the simulator or it did not work. My programmer cannot run on the processor. Narrow in the simulator remains green. I program the processor over the TBDML interface. I made the board myself and only program the processor I'm going to do.

My target is CAN bus over XGATE.
I would ask someone if someone would send me an e-mail with a program on XGATE.

And are XGATE and CPU working interrupts together. CPU serves internal interrupts (for example timers T0,T2 and sci) and XGATE serves only CAN ... I think, thet it will do, because I am going to determine interrupts in XGATE ??? Change XGATE Vector-tables ...

Thank you so much

email: [email protected]

0 Kudos
Reply
2 Replies

1,237 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

have you seen the examples I put on community?

LAMA's S12XE unofficial examples 

Some more can be find at:

https://community.nxp.com/docs/DOC-95116 

If you still have issue do not hesitate to ask.

Best regards,

Ladislav

0 Kudos
Reply

1,237 Views
lubošvidner
Contributor I

Hi, lama

No, I have not seen it. I am looking at it.

Thanks a lot.

0 Kudos
Reply