Use the S12ZVML-MINIBRD Board to change the motor speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use the S12ZVML-MINIBRD Board to change the motor speed

ソリューションへジャンプ
1,332件の閲覧回数
519315342
Contributor I

Can I modify the code to change the motor speed?

what is the code to control the speed of the motor ? And how to modify the code can control the motor speed?

ラベル(1)
0 件の賞賛
返信
1 解決策
999件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,000件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

0 件の賞賛
返信