Use the S12ZVML-MINIBRD Board to change the motor speed

cancel
Showing results for 
Search instead for 
Did you mean: 

Use the S12ZVML-MINIBRD Board to change the motor speed

Jump to solution
552 Views
519315342
Contributor I

Can I modify the code to change the motor speed?

what is the code to control the speed of the motor ? And how to modify the code can control the motor speed?

Labels (1)
0 Kudos
1 Solution
219 Views
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

View solution in original post

0 Kudos
1 Reply
220 Views
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

0 Kudos