The floating point type was not selected when the project was built. Can it be added in the future?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The floating point type was not selected when the project was built. Can it be added in the future?

Jump to solution
978 Views
maxxu
Contributor IV

hi!

   I use code warrior10.7 to built a new project,but forget setting floating point options ,Can it be added in the future?

  S912ZVM

0 Kudos
Reply
1 Solution
905 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Max,

You can enable floating-point by right click on your project -> Properties and after that select appropriate librarypastedImage_1.png

This question was already discussed in the community, for example, in the link below. I recommend you to read a Note where are described ANSI libraries, it helps you to select the right one.

https://community.nxp.com/message/849209?commentID=849209#comment-849209 

Best Regards,

Diana

View solution in original post

1 Reply
906 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Max,

You can enable floating-point by right click on your project -> Properties and after that select appropriate librarypastedImage_1.png

This question was already discussed in the community, for example, in the link below. I recommend you to read a Note where are described ANSI libraries, it helps you to select the right one.

https://community.nxp.com/message/849209?commentID=849209#comment-849209 

Best Regards,

Diana