SCI send decimal zero not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCI send decimal zero not working

3,018 Views
devarajraj
Contributor I

I am trying to work with SCI on the uC MC9S12XHY256 and seem to set right baud rate of 9600 and I think my initialization is correct. If i send char ‘A’, 'B' and decimal value 1 is working. I send decimal zero or null char is not working.

Does anyone have an idea?

Labels (1)
0 Kudos
Reply
5 Replies

2,826 Views
devarajraj
Contributor I

Hi Daniel,

Thank you for your support.
I want to send sensor value for 4 digits and my requirement is only two bytes.
how to transmit in SCI?

Ex: I send sensor value 3245

Transmit side:
int16 sensor_val = 3245
char buffer[2];
buffer[0]=sensor_val /256
buffer[1]=sensor_val %256

if i send sensor_val = 280
buffer[0]=1
buffer[1]=24

if i send sensor_val =240
buffer[0]=0
buffer[1]=240

Receiver side :
int8 getdata,getdata1;
int16 sensorout;

getdata = buffer[0];
getdata1 = buffer[1];

sensorout = (getdata *256+getdata1 )
sensorout = 3245

Regards

Devaraj

0 Kudos
Reply

2,826 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Use bit shift:

 

uint16_t  sensor_val = 3245;

uint8_t sensor_val_low, sensor_val_high;

 

sensor_val_low  = (sensor_val & 0xFF);
sensor_val_high = (sensor_val >> 8);

buffer[0]= sensor_val_low;  
buffer[1]= sensor_val_high;

 

And the other way round on the other site.

 

uint16_t sensorout;

uint8_t getdata_low, getdata_high;

getdata_low = buffer[0];

getdate_high = buffer[1];

 

sensorout = (getdata_high << 8);

sensorout |= getdata_low;  

Regards

Daniel

 

0 Kudos
Reply

2,826 Views
martynek
Contributor II

Hi

If you want to send decimal 0, send 0x30 (ASCII).

arr[1] = 0x30;

PutChar1(arr[1]);

 

Regards

 

Daniel

0 Kudos
Reply

2,825 Views
martynek
Contributor II

Hi

Could you provide us the code?

Note: In case a resource(s) cannot be publicly shared on Community, use the following procedure.

Regards

Daniel

0 Kudos
Reply

2,826 Views
devarajraj
Contributor I

Hi,

The attached code is what i am using to try to send data out the SCI port.The problem that no response for decimal zero on the output window(hyper terminal). code:

void SCI_Config(uint16 prescaler)
{
SCI1BDH = (uint8)((prescaler>>8));
SCI1BDL = (uint8)(prescaler);
SCI1CR1 = 0x00;
SCI1CR2 = 0x2C;
}

void PutChar1(uint8 ch)
{
while(!SCI1SR1_TDRE) {};
SCI1DRL = ch;
}

void main(void)
{
Clock_Init();
SCI_Config(156);
EnableInterrupts;
arr[0] ='A';
arr[1] = 0;
arr[2] = 'B';
PutChar1(arr[0]);
PutChar1(arr[1]);
PutChar1(arr[2]);
for(;;)
{
}
}

EXample:
Input
arr[0] ='A';
arr[1] = 0;
arr[2] = 'B';
output
A B

Thank you,

Regards,

Devaraj 

0 Kudos
Reply