ZVC bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZVC bootloader

1,846 Views
xiaohui200808
Contributor III

Hello

     I make a bootloader on one project.In app I donot use the interrupt .It could work normal (include update app).But when my app use the interrupt .I relocated the interrupt table.when I download it By Multilink .app(boot and app are in one project ) could work normally. But when I update the app ,it can not work normally .I read the Flash ,the S19 which I download ,are right .when  reloacated the interrupt table ,need there something to prepare. Attenchment is my code .Please help me check it . 

Original Attachment has been moved to: New_S12ZVC_Boot123.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,534 Views
RadekS
NXP Employee
NXP Employee

Hi Xiaohui,

Please look at our conversation in your previous thread:

https://community.nxp.com/message/870851

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply