S912XEG128J2CAA  example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912XEG128J2CAA  example code

3,497 Views
froggy
Contributor I

Dear all,

I have bought  S912XEG128J2CAA,  QFP 80.

I am looking for examples how to initialize MCU module.

Labels (1)
7 Replies

3,236 Views
iggi
NXP Employee
NXP Employee

Hi,

Here you can find many examples:

S12X Examples Pack 

LAMA's S12XE unofficial examples 

The Code Warrior projects are made for S12XEP100 device which is the top of S12XE MCU line.

You can take the main code from these projects and use it in your new CW project created for S12XEG128 device.

I hope this would be of help.

Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,236 Views
froggy
Contributor I

Thank you for your reply.

I cannot download the file--S12XE-001.ZIP.

Would you pease send me the file by email?

many thanks!

Have a nice day!

0 Kudos
Reply

3,236 Views
iggi
NXP Employee
NXP Employee

Hm... that file is not available as it has been deleted somehow.

We will fix it asap and inform you.

Regards,

iggi

0 Kudos
Reply

3,236 Views
xingqiufu
Contributor I

Hello Iggi,

Is the issue of S12XE-001.ZIP fixed now? Thanks.

Best regards

Xingqiu FU

0 Kudos
Reply

3,236 Views
iggi
NXP Employee
NXP Employee

The problem is still active. We tried to fix it, but no success. It looks like community system blocks it.

0 Kudos
Reply

3,236 Views
xingqiufu
Contributor I

Thanks Iggi. Could you please share me the examples related to freemaster as follows per email?

XEP100-FREEMASTER-BDM-CW50.ZIP

XEP100-FREEMASTER-SCI-CW51.ZIP

XEP100-FREEMASTER-test-CW47.zip

Best regards

Xingqiu Fu

0 Kudos
Reply

3,236 Views
iggi
NXP Employee
NXP Employee

Here are the examples packed in compressed folder. Inside you will find guidance in word doc. I've tested it on FreeMaster 2.0 and it works.

0 Kudos
Reply