S12ZVM ADC timing and data consistency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM ADC timing and data consistency

3,931 Views
lill1990
Contributor I

Dear sir,

I have a code fragment as below in my application. 

/*****************************************************************/

ADC0FLWCTL_RSTA = 1u;

while (ADC0CONIF_1_EOL_IF == 0u) 
{
//_asm("NOP");
Variable1= ADCResult[0];  /*read data from RVL*/
Variable2= ADCResult[1];
}

/*****************************************************************/

When the loop is exited(all ADC commands were completed, EOL_IF was set), I could get valid Variable1, however, the Variable2 was mostly invalid.  

I inserted a  "NOP" to the loop, then I could get all data.

I suspect it is caused by ADC timing and data consistency, but I don't have a clear understanding about that.

Could you tell me the probably reason behind this ?

Thanks very much.

0 Kudos
Reply
7 Replies

3,925 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @lill1990,

As per the EOL_IF description, this bit is set by the binary coded conversion command type select bits CMD_SEL[1:0] for “end of list” type of commands and after such a command has been processed and the related data has been stored RAM.

Can you share the whole ADC configuration?

Or a test project so that I can reproduce the error?

 

Thank you,

BR, Daniel

 

 

0 Kudos
Reply

3,918 Views
lill1990
Contributor I

Hello Daniel,

Thanks very much for your reply.

I attached the code and hope it is helpful for you.

0 Kudos
Reply

3,913 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Thank you for the code.

I see you use the max specified BUS_CLK freq (50MHz) and ADCCLK freq (8.33MHz).

Which PLL mode do you use?

Are you sure the BUS_CLK = 50MHz?

Can you scope the clock at ECLK?

Is PLL modulation enabled (CPMUPLL)?

 

Thanks,

Daniel

 

 

 

0 Kudos
Reply

3,906 Views
lill1990
Contributor I

Hello Daniel.

IRC is used in my application and I am sure the clock is correct.

PLL frequency modulation is off.

Thanks.

0 Kudos
Reply

3,899 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @lill1990,

I will need to test it.
What is the part number of the MCU (mask-set)?


From the code, I see that you measure the VSUP only if VSUP < 4.5V
Have you tested it under normal conditions when VSUP =~12V.

Since the measurement takes place at low supply voltage, is the BUS_CLK (ADC_CLK) stabilized at the time of the measurement?

Thanks,
Daniel

 

0 Kudos
Reply

3,895 Views
lill1990
Contributor I

Hello Daniel,

The MCU is MC9S12ZVML31, mask set 1N14N.

Yes, the code is used in the initialization to ensure the VSUP is >=4.5 before starting GDU.

The VSUP was stable as 12V, I reset MCU to test this function via debugger.

I tried to add a breakpoint into the while{ADC0CONIF_1_EOL_IF == 0u} loop, then continue running, every thing was OK. I think the ADC completed the conversation during the break.

But if no any break before EOL flag was set by HW, the behavior I described in this question will appear.

Thanks.

0 Kudos
Reply

3,826 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @lill1990,

I'm sorry for the delay, I was out of office for a few days and could not test it earlier.

I'm not able to reproduce the issue with the test code attached.

Can you run the test project on your side?

 

BR, Daniel

0 Kudos
Reply