S12XEP100 Reset Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12XEP100 Reset Issue

5,000 Views
dannydeng
Contributor III

Dears,

   Our customer use MC9S12XEP100MAG for Automotive Power Controller, and now find some times software run stuck, at this moment, we can not reset via Hiwave.exe when Hysnatic. Also, can not reset by short RST, GND.

Ray

BRs,

0 Kudos
Reply
5 Replies

4,832 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

It is not easy to answer your issue. This is not a standard behavior. As a first step I would like to see the schematic design of the MCU environment. If it is confidential please create a case via support pages or I can do it in behalf of you. Of course, the device can be damaged from any reason.

MCU reset is independent from any HW/ SW or structure inside the MCU. In the “application” (normal) mode of the MCU it can happen you are in permanent circulating Reset because of incorrect SW but if you are not able to reset externally via hiwave it is an issue. I hope, you have, in order to be sure, MODC pulled up, MODB and MODA pulled down to be able to generate special single chip mode. One thing I would also to check is, I would start the MCU in special single chip mode MODC=MODB=MODA=0 and check XCLKS pin whether the MCU is running. You should see BUSCLK=OSCCLK/2 at the ECLK pin.

Best regards,

Ladislav

0 Kudos
Reply

4,832 Views
dannydeng
Contributor III

Hi Ladislav,

Thanks for your kindly help,

I did HotSync in the same software position,found the data difference as attached, can you help to advice?

Thanks & Best Regards.

Ray Deng (邓成平)

Tel: (086)0755 8250 5493

Mobile: 180 2696 0272

发件人: lama <[email protected]>

发送时间: 2019年8月1日 16:14

收件人: Ray Deng <[email protected]>

主题: Re: - Re: S12XEP100 Reset Issue

CAUTION: This email originated from outside of the organization. This message might not be safe, use caution in opening it. If in doubt, do not open the attachment nor links in the message.

NXP Community <https://nam04.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Cray.deng%40arrowasia.com%7C2bfc53497c0f42e037b408d716582b38%7C0beb0c359cbb4feb99e5589e415c7944%7C1%7C0%7C637002440251095954&sdata=Jo9GVAaR7Rz0bX1ucl1EwohDmLBglKU6FIJHE8e8Yxs%3D&reserved=0>

Re: S12XEP100 Reset Issue

reply from lama<https://nam04.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2Flama%3Fet%3Dwatches.email.thread&data=02%7C01%7Cray.deng%40arrowasia.com%7C2bfc53497c0f42e037b408d716582b38%7C0beb0c359cbb4feb99e5589e415c7944%7C1%7C0%7C637002440251095954&sdata=bZAm48xpqHXBsBcxWAqCCilBeyDxKeXAtbc%2FolCnSCs%3D&reserved=0> in S12 / MagniV Microcontrollers - View the full discussion<https://nam04.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1185929%3FcommentID%3D1185929%26et%3Dwatches.email.thread%23comment-1185929&data=02%7C01%7Cray.deng%40arrowasia.com%7C2bfc53497c0f42e037b408d716582b38%7C0beb0c359cbb4feb99e5589e415c7944%7C1%7C0%7C637002440251105950&sdata=D5nIGAEH%2FTb8CQfS2rMUxw5GksGN37fHrKy%2B%2BtRhEkQ%3D&reserved=0>

0 Kudos
Reply

4,832 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I am sorry I was out of PC for a few days. Is the issue still active?

Best regards,

Ladislav

0 Kudos
Reply

4,832 Views
dannydeng
Contributor III

Hi Lama,

   Thanks for your kindly help,

   The problem is sitll sticking us,customer used uCOS in their system, when stuck, Hiwave software reset or hardware jump reset to GND can not change the MCU registers status, only reboot via power off can help to work well.

  Can you help to advice?

BRs,

Ray

0 Kudos
Reply

4,832 Views
lama
NXP TechSupport
NXP TechSupport

I sent you a message via another connection. I would like to continue via that connection for a moment. Finally we can put solution back here.

best regards,

Ladislav

0 Kudos
Reply