LTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTC

2,154件の閲覧回数
cui1
Contributor II

I was reading the MM9Z1J638 data book and found the LTC module. I want to know what he's for.

0 件の賞賛
返信
3 返答(返信)

2,090件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 


6.2.2.4.1.5Wake-up on life time counter overflow
The life time counter continues to run during Low-power mode, if configured. Once the counter overflows with the life time counter wake-up enabled (WULTC=1), a wake-up is issued. The wake-up source is flagged with the WULTC Bit. The Life Time Counter has to be configured in Normal mode only.


WULTCF
Life Time Counter Wake-up Flag. Writing this bit to logic 1 will clear the flag.
0 - n.a.
1 - Last Wake-up was caused by a life time counter overflow

Best regards,

Ladislav

0 件の賞賛
返信

2,132件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

The timer ca be used for anything you want. The primary design purpose was to provide independent timer which can store running time when the MCU is running. Some customers required it to be able to check running time without stealing another peripheral.

 

Best regards,

Ladislav

0 件の賞賛
返信

2,104件の閲覧回数
cui1
Contributor II
Hello then can I use it as a low power sleep or stop and use it as a wake source. thanks!
0 件の賞賛
返信