What is the accuracy of the frequency deviation of the crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the accuracy of the frequency deviation of the crystal

ソリューションへジャンプ
1,133件の閲覧回数
yq1
Contributor III

Hello, 
I would like to know that when the external crystal of S9S12G128F0MLF is 16MHz.
What is the accuracy of the frequency deviation of the crystal to meet the requirement of CAN communication?

 

thanks

0 件の賞賛
返信
1 解決策
1,118件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

There is https://www.nxp.com/docs/en/application-note/AN1798.pdf

Moreover you can use my calculator …. CAN_setup9.xlsx … attached.

The result for oscillator precision is in the cell results-> required oscillator tolerance [%]

Moreover, this require to be oscillator used as a CAN clock (not bus clock generated from PLL)

Some CAN examples you can find attached.

Best regards,

Ladislav

元の投稿で解決策を見る

1 返信
1,119件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

There is https://www.nxp.com/docs/en/application-note/AN1798.pdf

Moreover you can use my calculator …. CAN_setup9.xlsx … attached.

The result for oscillator precision is in the cell results-> required oscillator tolerance [%]

Moreover, this require to be oscillator used as a CAN clock (not bus clock generated from PLL)

Some CAN examples you can find attached.

Best regards,

Ladislav