Is microcontroller S9G64CF0 the same as S9S12G64F0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is microcontroller S9G64CF0 the same as S9S12G64F0?

跳至解决方案
1,355 次查看
luis366
Contributor I

Hello,

I have several PCB Assemblies from work that contain a Freescale microcontroller with the PN S9G64CF0N75C printed in their body. 

Is this the same PN as 9S12G64F0C? (I have been only able to find documentation on this MC9S12G Family of micros.

Thanks

Luis Mendez

0 项奖励
回复
1 解答
1,337 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

They are the same. There is only change in a numbering where the mask set is included into a part number as a code F0.

S9G64CF0N75C …. I suppose you have missed “L” and it should be S9G64CLF0N75C. (0N75C is a a mask set 75C of revision 0)

9S12G64F0C? ….. 9S12G64F0CLF, 9S12G64F0CLFR : F0 = Mask set 0N75C; R=Rape&Reel; LF=48 LQFP; C- -40~85deg.C.

There is confusing combination of letters F0.
In the first case it should be understood S9G64CLF 0N75C
In the first case it should be understood S9G64F0CLF

Best regards,

Ladislav

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,338 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

They are the same. There is only change in a numbering where the mask set is included into a part number as a code F0.

S9G64CF0N75C …. I suppose you have missed “L” and it should be S9G64CLF0N75C. (0N75C is a a mask set 75C of revision 0)

9S12G64F0C? ….. 9S12G64F0CLF, 9S12G64F0CLFR : F0 = Mask set 0N75C; R=Rape&Reel; LF=48 LQFP; C- -40~85deg.C.

There is confusing combination of letters F0.
In the first case it should be understood S9G64CLF 0N75C
In the first case it should be understood S9G64F0CLF

Best regards,

Ladislav

 

0 项奖励
回复