Interfacing two MC9S12XEP100 using CAN MAX3050 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface

1,838件の閲覧回数
harshal_pawar
Contributor III

I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.

Is there any sample code available for the same as per your protocol standards?

ラベル(1)
2 返答(返信)

1,714件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Harshal,

The application note AN3034 was recommended to you in your first case 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface 

I can also recommend you to the MSCAN driver for the S12(X) devices:

MSCAN S12 driver 

I hope it helps you.

Best Regards,

Diana

1,714件の閲覧回数
harshal_pawar
Contributor III

Thanks

0 件の賞賛
返信