Interfacing two MC9S12XEP100 using CAN MAX3050 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface

1,342 次查看
harshal_pawar
Contributor III

I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.

Is there any sample code available for the same as per your protocol standards?

标签 (1)
2 回复数

1,218 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Harshal,

The application note AN3034 was recommended to you in your first case 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface 

I can also recommend you to the MSCAN driver for the S12(X) devices:

MSCAN S12 driver 

I hope it helps you.

Best Regards,

Diana

1,218 次查看
harshal_pawar
Contributor III

Thanks

0 项奖励
回复