I need IBIS file of MC9S12H,but I can't find it on NXP website.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need IBIS file of MC9S12H,but I can't find it on NXP website.

1,694 Views
michaelvon
Contributor I

I am an electrical Engineering student.I need the IBIS model of MC9S12H for some simulations,but I found nowhere to download it after five-hours searching.So I'm asking for the IBIS model of MC9S12H MCU chip,or other HCS12 family ones.would be very grateful.

 

Thanking in advance.

Best Regards,

Michael Von

Labels (1)
0 Kudos
Reply
4 Replies

1,397 Views
iggi
NXP Employee
NXP Employee

Dear Micheal,

unfortunately we do not have IBIS model for S12H device family. as well as for other MCU families based on 0.25um technology. There is IBIS model for S12XE device family which is the top of the S12(X) line, but this MCU is based on 0.18um technology and so the document would not be much of help.

Regards,

iggi

0 Kudos
Reply

1,397 Views
michaelvon
Contributor I

Dear iggi ,

Thank you very much! I think the IBIS model for S12XE could help me at least, but I found nowhere to download that IBIS file. Could you please give me a link?

(Sorry for my replying late, I have not found the Reply button until today.)

0 Kudos
Reply

1,397 Views
iggi
NXP Employee
NXP Employee

Micheal,

i am not sure if i can share the IBIS file publicly. Can you please open a ticket for this case?
https://community.nxp.com/docs/DOC-329745 

There are several steps and registration is needed, but i hope that's ok.

Regards,

iggi

0 Kudos
Reply

1,397 Views
michaelvon
Contributor I

Dear iggi,

Thank you for your detailed explanation. I will follow the steps.

Regards,

Michael

2016-11-14

f_huiyuan

发件人:iggi <admin@community.nxp.com>

发送时间:2016-11-14 22:03

主题:Re: - Re: I need IBIS file of MC9S12H,but I can't find it on NXP website.

收件人:"Michael Von"<f_huiyuan@163.com>

抄送:

NXP Community

Re: I need IBIS file of MC9S12H,but I can't find it on NXP website.

reply from iggi in S12 / MagniV Microcontrollers - View the full discussion

Micheal,

i am not sure if i can share the IBIS file publicly. Can you please open a ticket for this case?

How to submit a new question for NXP Support

There are several steps and registration is needed, but i hope that's ok.

Regards,

iggi

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S12 / MagniV Microcontrollers by email or at NXP Community

Following Re: I need IBIS file of MC9S12H,but I can't find it on NXP website. in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply