How to use S12Z to measure motor phase voltage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use S12Z to measure motor phase voltage?

860 Views
jiangfeng
Contributor III

Dear support:

I use the S12Z to drive the motor and try to detect the phase voltage, Is the pin(HS0 HS1 HS2) used to detect the phase voltageA,B,C?

pastedImage_3.png
Is the phase voltage described above correspond to Ua,Ub,Uc in the following figure? Thanks very much.

pastedImage_2.png

0 Kudos
Reply
1 Reply

714 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Yes, see GDUPHMUX register.

Please refer to the application note:

http://www.nxp.com/docs/en/application-note/AN4704.pdf 

All our solutions for S12ZVM motor control are listed in the document below:

https://community.nxp.com/docs/DOC-334960 

Regards,

Daniel

0 Kudos
Reply