CSMB-12XDT512 on 64 bit windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSMB-12XDT512 on 64 bit windows

1,014件の閲覧回数
carlsmith
Contributor I

I have a CSMB-12XDT512 and since I have a 64 bit computer I cant get it to debug on with FreeScale V5.1 software with just a USB cable that I could once do with windows 32 bit and I know you have to use a USB BDM Pod but the 6 pin BDM on my board has no pins, am I supposed to solder some on it? Has someone already had this problem and did it work?

0 件の賞賛
返信
1 返信

944件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Yes, unfortunately, TBDML interface drivers are not supported on 64bit OS.

You can use the BDM interface, for instance P&E USB Multilink, you will need to mount the BDM port. 

Or you can use a virtual 32bit PC, as it is explained in AN3936.

Regards,

Daniel

0 件の賞賛
返信